I am using LMR43620MSC3RPERQ1. On the page 38 of datasheet, it states "If the application is operating close to the minimum input voltage, this dip can cause the
regulator to momentarily shut down and reset. The best way to solve these kind of issues is to limit the distance
from the input supply to the regulator or plan to use an aluminum or tantalum input capacitor in parallel with the
ceramics. The moderate ESR of these types of capacitors help dampen the input resonant circuit and reduce
any overshoots. A value in the range of 20 μF to 100 μF is usually sufficient to provide input damping and help to
hold the input voltage steady during large load transients.".
My power input is 5V (USB port) and output is 3.3V. The trance length is less than 25mm. Should I still add an aluminum cap? I have a concern on vibration profile on the aluminum cap and the tantalum cap is too expensive. Thank you.
Rong