Other Parts Discussed in Thread: TPS22950
Hi Team,
I have three questions about TPS22953:
1. Does TPS22953 have over current protection feature, if yes, what's the limited current value (5-A Maximum Continuous Switch Current)
2. The power good pin is related to VEN and VSNS, seems it only monitors the input and output voltage level. Can this pin indicates the over current status?
3. In datasheet WSON package type has two package drawing types, both are Ok for customer or which one is the suggested choice.
Appreciate for your technical replay and Thanks in advance
BR
Steven