This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217: na

Part Number: TPS65217

Can I use the function of charging the external battery and using the external battery to power up other circuitry when not in charging mode.

  • Hi Cindy,

    Thanks for reaching out. As stated in the datasheet, the input power source for charging the battery and running the system can be either an AC adapter or a USB port. The system (VSYS pin) can be powered by AC, USB or Battery but the power path will prioritize AC input over the USB input, and both over the battery input. The battery will be used to supply the system only when AC and USB are not present. This feature makes sure the AC and USB supplies are used whenever possible to save battery life. 

    Please refer to section "Battery Charger and Power Path" in the datasheet for more information and let me know if you have additional questions. 

    Thanks,

    Brenda

  • do you have an schematic sample on how I should connect?

  • thanks for the fast response, can I also check that when there is no AC and USB i understand that battery will take over.

    while powering up my device using the battery can i choice on which regulator to power up to minimise current drawn from battery?

  • Hi Cindy,

    The figure below shows the recommended connections for the power path. This information can be found in the Brownout report.

    Here I'm listing some links with more information in addition to the datasheet which can be used as a reference when designing with TPS65217. 

    The datasheet and additional documentation can be found under "Technical documentation" in the product folder at ti.com. 

    Thanks,

    Brenda