Other Parts Discussed in Thread: LM5121
Boost converter
Input : 5V
Output : 10V@ 6A
Switching frequency:450 Khz
Output ripple is observed around 400mV.After probing Switch node,Wide and narrow duty cycles observed alternately.
Changed the Rslope value as calculated from eqn 6 in datasheet Page:16
Still the issue is not solved.
Any other parameter to be re-looked for alternate wide and narrow duty cycles.Boost converter.pdf