Hi
I'm trying to simulate the scenario (with PSpice), when the Vcc is powered by Vout or other external DC source (8V - 13V).
I've downloaded the "LM5146-Q1 PSpice Unencrypted Transient Model (Rev. A)"
The only thing I've added are two diodes in series to Vin and Vcc as mentioned by datasheet:
As you can notice the Vcc stays at 7.5V while 12V supply produces output power of -10.8KW!!!
I've also tried to connect Vout instead of 12V, so the output voltage is stuck at approximately 7.5V instead of getting 12V.
Am I missing something in theory of operation? Can it be some problem of the simulation model?
Thanks a lot
Alex