This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62913: how to improve EMI radiation

Part Number: TPS62913

Hi,

In my board I use 3 devices from TPS62913 types.

How should I connect them to prevent as much as I can EMI issues?
First DCDC:
VIN = 9V; VOUT = 1V @ 1.5A

Second DCDC:
VIN = 9V; VOUT = 3.6V @1.3A

Third DCDC:
VIN = 9V; VOUT =5V@ 1A.

The first and second DCDC always on and the third selected with EN.

Can I sync them without external clock?

Thanks