Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM
Dear All,
We used the BQStudio to get the ChemID for our Li-ion Battery, we are using the BQ27510EVM with EV4200 to gather the log as required on the document http://ti.com/lit/slva725
We followed these steps:
- Started with an empty Battery.
- Charging the battery for 4 Hours (Without a load until the current dropped from 512mA to 0mA suddenly, and the voltage increased from 4.23V to 4.9 which is the charger output voltage)
- Relaxing for 2.19 Hours (Without a load)
- Discharging the battery for 7.6 Hours (With a load- the average current ranges between 450:550mA)
- Relaxing for 6.7 Hours
Taking into consideration that the battery capacity is 4000mAh, and charging voltage is 4.2V, discharging voltage is 3V (This information are listed on the datasheet of the battery)
The data log is available within this link DataLog
So we have some questions,
- Did we follow the instruction correctly since it's not clear if we need a load during relaxation and charging or not?
- During discharging, when do we consider that the discharging is completed, is it when we reach the termination voltage (3V) or when no current is drawn by the load (0A)?
Talking into consideration that we used the Gauging Parameter Calculator, and we got the following output
0 0 0 0 0
Warning: First OCVpoint has non-zero current I= 0.915 Please make sure you have a 2 hr relaxation period before the beginning of discharge. 0 0 0 0
Warning: Last OCVpoint has non-zero current I= 0.92 Please make sure you have a 5 hr relaxation period after the end of discharge. 0 0 0 0
Warning: Discharge rate is too high. High rate reduces ID detection accuracy 10 hr rate is recomeended. Total discharge time is less than 5 hrs t_hrs= -0.00138888888888889 0 0
Error: No discharge portion found Make sure discaharge current is negative N_points= 2 0 0
Looking forward to your reply.