Other Parts Discussed in Thread: TPS22913, TLV62150
Dear Team,
Our customer have a project with dual input .
They use TPS2121 for oring circuit.
Power input as the below.
- USB 5V@3A
2.Battery 6V~8.4V @2A
They hope default input is USB 5V when both input existing .
Please review the schematic. Thanks.
Jimmy