We are using mentioned device (LM26003) in one of our designs.
We would like to get the schematic reviewed before we move forward for manufacturing.
Below are the some parameters -
Max output current required: 2A
Input voltage range: 9V-24V
Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using mentioned device (LM26003) in one of our designs.
We would like to get the schematic reviewed before we move forward for manufacturing.
Below are the some parameters -
Max output current required: 2A
Input voltage range: 9V-24V
Thanks.

Hi Varun,
Yes, need to add one more 220pF from COMP to GND to limit the control loop bandwidth.
B R
Andy