Hi,
I'm performing capacitor derating analysis for some of our boards. I need to know the max operating voltage applied at the Bootstrap capacitor for LMR14203 and LM2842Y. Could you please let me know?
Thank you,
Komal Charan Garlapati
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm performing capacitor derating analysis for some of our boards. I need to know the max operating voltage applied at the Bootstrap capacitor for LMR14203 and LM2842Y. Could you please let me know?
Thank you,
Komal Charan Garlapati
HI
for LMR14203, 7V is max voltage between boot and SW, as SW will be Vin and -0.7V, so boot max voltage is Vin+7V,
for LM2842Y is same voltage rating with LRM14203
Hi Daniel,
Just wanted to confirm with you, the voltage across the capacitor (between SW and CB) is independent of Input or the Output voltage. It is for providing the sufficient drive voltage for the Gate Pin above the Source Pin. Am I right?
Also, the datasheet mentions that 7V is the absolute max voltage. So, the max working voltage shall be lesser than 7. Right?
HI
yes, it is independ of Output voltage and input votage unless Vin<5V, as the boot voltage won't higher than Vin.
The max working voltage is less than 7V,