I'm using the TPS613222A for my project and am referencing the datasheet for it, particularly figure 24. The data sheet says, in the device comparison table, that the typical current for the chip is 1.8 A. How can I adjust the parameters of the passive and active elements in figure 24 to get an output of 1 A, if my battery is 3.7 V (Nominal)? Please let me know if more information is needed for proper assistance.