In LM25118MH, an Input of 9V was given and an output of 28V has been generated.
We had done some experiments like connecting the other boards (Input voltage of 28V in 3 numbers)in parallel to the buck converter by tapping out
we had done power budgeting for the working board of 3 numbers(which is acting as an RLC load) it is not exceeding the maximum load current of the buck-boost converter.
But while connecting the first board, buck-boost can able to source the current.
Then we try tried to increase the load by hot plugging the second board. At this time we are observing that the Buck-Boost converter cannot able to source the current to the second board.
At the same time, we had tried with the pure resistive load, at the time current is sourced from the buck-boost converter
we are suspecting that it is due to the capacitive effect. due to the capacitive effect, Inrush current is more while doing the hot-plugging of the second board.
Is that a real reason behind that? or something else? what will happen internally in buck-boost converter