This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92390: Use by reducing the output of 4ch to 2ch

Guru 10445 points
Part Number: TPS92390

Hi,

TPS92390 is a product with 4ch output and maximum output current of 200mA x 4ch.

Is it possible to reduce this product from 4ch to 2ch output and use it as a maximum output current of 400mA x 2ch?

Thanks,

Koki