Other Parts Discussed in Thread: TPS63900
I ran across the TPS61094 because I have almost the exact setup of of the following TI article: https://e2e.ti.com/blogs_/b/powerhouse/posts/3-benefits-of-using-a-low-iq-buck-boost-converter-to-extend-battery-life-in-flow-meters. The main difference is that I need a constant Vout of 5V. Up until now, I've been running directly from battery and using a simple boost converter but after I read this article, I realized I needed to add the super cap to protect my battery from the high current draws that occur a couple of times a day when LTE-M is turned on.
I've read through the datasheet a few times and am trying to understand what would happen if in this diagram below, Vin and Vout reversed (Vin: 3.6V, Vout: 5V) while running in auto boost buck mode. If this were the case, would buck mode never occur and thus the super cap would never be used? If it is the case that the TPS61094 would do little in the area of battery preservation by utilizing a super cap, do you have other recommendations to achieve a similar setup (3.6V boosted to 5V while limiting high current draw on battery)?
Thanks