Hi team,
I have a question about Figure 12 on the datasheet. It shows the knee of VOUT=1.2V is around 0.25A, and 2.5V is around 0.15A, although IL reaches 0A when 0.14A at VOUT=1.2V, 0.2A at VOUT=2.5V respectively. I think it is opposite because delta_IL at VOUT2.5V should be larger than VOUT1.2V. If it's not true, please let me know the reason why.
Regards,
Kazuto