This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61199: Current Sink Inputs

Part Number: TPS61199

Hi,

Good Day. On page 16 of the datasheet(TPS61199) , customer see a schematic drawing showing us that two regulated current sink inputs could be connected to each other in order to double the current in the led streams. In his application he need a led current equal to 0.5A  and a VLed=53V for one stream . Is it possible to connect the 8 regulated current sink input to each other in order to have only one stream with a current = 0.5A.

Best Regards,

Ray Vincent