This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: Review

Part Number: LM5069

Copy of LM5069 Design Calculator_24V_1.xlsm385851-ADB (4-7-2022 3-35-05 PM).zip

Hi,

Please find the attached excel calculator and design files. Please do review the schematic for below inputs and let me know any changes required .

My inputs are as follows,

My assumptions for 24V input supply voltage are as follows,

Upper under voltage = 23V

Lower under voltage=22V

Upper over voltage=26V

Lower Over Voltage= 25V

I am going with Option B for Resistor calculations for Under and over voltage limit settings and please clarify what does makes difference with other options and when to use?

For Rsense calculation :

Rsns=Vclmin/Ilim

Vclmin=48.mV from Datasheet

And Ilim=1.2A Design requirement 

Then Rsns= 48.5mV/1.2A=40mOhm

kindly let me know my calculations and design is correct or any changes required.

Awaiting for your response 

Thanks & Regards

Chiranjeevi