Part Number: LM5069
Other Parts Discussed in Thread: TPS2597, TPS2596, TPS2595
Hi,
Please find the attached excel calculator and design files. Please do review the schematic for below inputs and let me know any changes required .
My inputs are as follows,
My assumptions for 24V input supply voltage are as follows,
Upper under voltage = 11V
Lower under voltage=10
Upper over voltage=14V
Lower Over Voltage= 13V
I am going with Option B for Resistor calculations for Under and over voltage limit
LM5069 Design Calculator_12V.xlsm385850-ADB (4-7-2022 2-02-39 PM).zip
For Rsense calculation :
Rsns=Vclmin/Ilim
Vclmin=48.mV from Datasheet
And Ilim=1.8A Design requirement
Then Rsns= 48.5mV/1.8A=26.68mOhm
kindly let me know my calculations are correct and for that circuit breaker will trip out of my limits.
Awaiting for your response
Thanks & Regards
Chiranjeevi