Other Parts Discussed in Thread: BQSTUDIO, , GPCCHEM, EV2400, BQ27426, BQ27510, BQ27510EVM
I need the debug address registers address location and definitions that are not documented in the datasheet or technical reference, but are available through Bqstudio. These registers are identified as Debug1, Debug2, Debug3, Debug4, Debug5, Debug6, and Debug7.
I need to identify how to read and interpret the coulomb counter to understand how much capacity is used when the state of charge registers zero out, and the device continues discharging above its termination voltage.
My interest is trying to determine when I have 30 minutes remaining of a higher discharge rate when the learning cycles and typical operations are done on a lower discharge rate.
Note: The full part number is: BQ27421YZFR-G1A
Thank you in advance for this information.