Dear E2E Forum,
I need to use LM5146-Q1-EVM12V.
I need minro modification as per my requirement given below:
- I/p on this card supports only 15V-85V DC but, my requirement for I/p is 45V-95V DC. So can i use it? what modification do i need to do for the same
- O/p on card is 12V upto 8A. but my requirement is o/p 12V 9A. So again can i use it? what modification do i need to do for the same?
Thanks in Advance.
Deeply awaiting your reply.