Part Number: BQ78350-R2-DEVICE-FW
Hello
a 7S 2P battery pack of ours is designed for a customer application.
In that application there is a big capacitor 1000mF and 63V connected to the battery terminals. Sometimes, by inserting a battery placed in ship mode in the system, the battery is awaken upon insertion because the capacitor, still with some load, generate a charge pulse enough to be detected as a wakeup condition.
Question: is it possible firmware wise to setup a delay so that the wake condition need to be applied for a certain minimum time ?
Thank in advance
Pietro