This thread applies to the power estimator for TPS65381A-Q1.
Attached is a updated version of the TPS65381 power estimator.
TPS65381A-Q1 Power Estimator - E2E FAQ.xlsm
The user can input the supply voltage (VBAT), the configuration voltages for VDD3/5, VDD1 and VSOUT1, the supply source for VSOUT1 (VDD6 or VBATP), load currents for the regulators, Vf of the diode, DCR of the inductor. As the user enters these inputs into the yellow cells with blue font the power estimated for the device will be calculated.