This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62177: FB Pin connections

Part Number: TPS62177
Other Parts Discussed in Thread: TPS62175,

We'd like to use the TPS62177 as a drop in replacement for the TPS62175. To make it as simple as possible, we'd like to leave the circuit for the TPS62175 in place, so FB would remain connected to the output. We're using a 402kohm resistor from FB to VOUT and 604k resistor from FB to GND. Based on the datasheet, the FB pin is fully disconnected from the circuit, except for a high value resistor to GND. 

Can you confirm that there's no other internal connection from FB to the circuit that may cause an issue if we leave the voltage divider in place?