This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6735: CS0976205 has been Updated - TPS6735IDR

Part Number: TPS6735

Need below information urgently,

1> Declaration Elements - Application Scenario

2>Declaration Elements - Capacity

Supplier

Supplier Name

Item Code

Mfg Partno.

Declaration Elements - Application Scenario

Declaration Elements - Capacity

ECCN

SPZU15030

Texas Instruments China Sales Limited

TEKH-K-IC-1588

TPS6735IDR

-

-

EAR99

  an example for reference given bellow.

Declaration Elements - Application Scenario


Declaration Elements - Capacity

ECCN

 

 Memory Chips > FRAM

  

64Kbit

EAR99

      

  • Hi,

    Thank you for posting, but we are BCS product line Apps team and what exactly do you need?   Regarding the applications of the TPS6735, is supports applications where a -5V regulated voltage rail is required but only  a positive voltage source is available in the system.  So it can produce the -5V rail from the positive voltage rail.  

    Hope this answers your question.

    Thanks,

    Youhao