The LM5116-12EVAL board uses a 10uH inductor.
i used the formula in the LM5116 datasheet (page 23) and used these values:
VinMAX = 80V
Vout = 12V
Ipp = 2A
fsw = 250000 Hz
The result is around 20uH
10uH would result in around 4A of ripple current.
According to the datasheet , the coil ripple should be between 20-40% if Iload.
Why is there a 10uH inductor used on that board ?