Hi Team,
Suggest TI solution and verify if it’s P2P compatible with MC7815BDTRKG from ON
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Victor,
Here are all the p2p solutions (minus TPS7A45).
|
MC7800 |
TPS7A45 |
LM2940C |
LM2940-N |
LM340 |
TL780 |
AEC Q100 |
NO |
NO |
NO |
NO |
NO |
NO |
Output Options |
Fixed Output |
Adjustable Output, Fixed Output |
Fixed Output |
Fixed Output |
Fixed Output |
Fixed Output |
Iout (Max) (A) |
1 |
1.5 |
1 |
1 |
1.5 |
1.5 |
Vin (Max) (V) |
35 |
20 |
26 |
26 |
35 |
30 |
Vin (Min) (V) |
7 |
2.1 |
6 |
6 |
7.5 |
7 |
Vout (Max) (V) |
24 |
20 |
15 |
15 |
15 |
15 |
Vout (Min) (V) |
5 |
1.5 |
5 |
5 |
5 |
5 |
Fixed Output Options (V) |
5, 6, 8, 9, 12, 15, 18, 24 |
1.5, 1.8, 2.5, 3.3 |
5, 9, 12, 15 |
5, 8, 9, 10, 12, 15 |
5, 12, 15 |
5, 12, 15 |
Enable |
NO |
YES |
NO |
NO |
NO |
NO |
Power Good |
NO |
NO |
NO |
NO |
NO |
NO |
Output Capacitor Type |
Non-Ceramic |
Ceramic |
Non-Ceramic |
Non-Ceramic |
Cap Free, Ceramic |
Cap Free, Ceramic |
PSRR @ 100KHz (dB) |
- |
38 |
54 |
48 |
50 |
- |
Noise (uVrms) |
240 |
35 |
150 |
150 |
40 |
75 |
Accuracy (%) |
4 |
2.5 |
5 |
2 |
2.5 |
1 |
Vdo (Typ) (mV) |
2000 |
300 |
500 |
500 |
2000 |
2000 |
Iq (Typ) (mA) |
3.2 |
1 |
10 |
10 |
8 |
5 |
Thermal Resistance θJA (°C/W) |
15 |
28 |
23 |
23 |
24 |
23 |
Min Package Area (mm2) |
40.14 |
45.89 |
46.5328 |
16 |
45.5 |
88.392 |
Package Type |
TO-220, TO-252, DDPAK/TO-263 |
DDPAK/TO-263, SOT-223 |
DDPAK/TO-263, TO-220, TO-220 |
DDPAK/TO-263, SOT-223, TO-220, WSON |
DDPAK/TO-263, SOT-223, TO-220, TO-220 |
DDPAK/TO-263, TO-220 |
Thanks,
McKyla