Hi,
please see the problem with BQ24171RGYT
we are using to recharge Li-Ion Battery of capacity 11.V(3S3P) and 6.6AH.
Adapter Power is 12.6V,current is 1.5A
Battery needs to be charged with CV at current rate of 1A.
Calculation is done as per the above ratings ,please see attached schematic for the same.
VACSET is set at 0.3V,OVPSET is set at 1V,VISET is set at 0.2V
our problem is Battery side SW (pin no 24 in the IC) is showing short to GND, even we have kept fast switching Diode for SW pin
please suggest are we doing any wrong ?