Hi,All.
Can a boost voltage appear on the pins when TPS60240 fails?
If so, is the upper limit of the boost voltage that appears on the external pins at the time of failure structurally determined?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,All.
Can a boost voltage appear on the pins when TPS60240 fails?
If so, is the upper limit of the boost voltage that appears on the external pins at the time of failure structurally determined?
Hi,
Thank you for posting. By "boost voltage" do you mean an upstream boost converter? It depends how the part fails. If the pin fails to ground, you may short the boost output and damage if there is no overloading protection. Note that a boost converter does not have natural mechanism to protect against output short.
Thanks,
Youhao
Hi Youhao,
I mean "boosted voltage" by higher voltage greater than supply voltage.
Among the answers to "TPS60240: Step-Down Operation", there was a part of "The Device Is Permanently Operating As Voltage Doubler".
e2e.ti.com/.../tps60240-step-down-operation
Is this device a structure that does not perform boosting operation other than as a voltage doubler, even in the event of a failure?
Do the eight pins of this device have an operating mode or failure mode that causes a voltage that is more than twice the supply voltage?
Hi,
It depends how the device fails. However, in the voltage doubler, the boost voltage can only be produced when the circuit is switching normally. At this moment we don't have a pin failure mode summary to share, but if the circuit fails, I would not expect the circuit could produce twice the supply voltage.
Thanks,
Youhao