Other Parts Discussed in Thread: UCC256404, , UCC28782
Hello Jaden:
Problem!
I tried to massage the Lr. Cr, Lm values in the UCC256404 design calculation Spreadsheet but it seems there is no convenient practical values one can obtain in this topology with high turns ratio & low power.
I see Lr in 500uH range, Cr approx 1nF, Lm 3000uH....Then Vcr may be 3000V!
These values will not make a consumer /industrial grade module at a convenient price range.
So I got to take another look at UCC28740.
As you had suggested earlier.
I will post if I find a way to proceed with LLC given that I bought out the Eval board, 100 PC of the controller etc!\LOL
We do have a project to make LLC modules...not right now.
Do you have some other controller? But for now, going to take another calculation for UCC28740. For input to 6500V, 5v output, 30-40W load.
Let us see where it goes from here.
Any help in this matter will be highly appreciated.
r