Using your TPS61094 component I am having problems with the buck function.
To better understand I bought the TPS61094EVM-066 evaluation board but without getting results.
By programming the "Auto Buck or Burst" function, as long as the input voltage is less than or equal to the output voltage, I get the required output voltage; when the input voltage exceeds the required output voltage, the output voltage follows the input voltage.
I have to supply 3.3V to the circuit using a 3.7V lithium battery and therefore I have to have the desired voltage with both a 4V and 2.7V input.
I need help.
Thanks.