Part Number: BQ78350-R2-DEVICE-FW
Hello,
we have a battery pack for a special power tool where the bq78350 is set with an IPSCALE of 0x1 (the current is scaled by 10mA).
The Current deadband is set to 1, so we can read the SBS.Current with a granularity of 10mA.
The Sleep Current is set to 2, so If I understand well any current below 20mA cause the evice to go to SLEEP MODE.
If the device to which thw battery is connected drains something like ~5mA, I expect the battery do not detect it and coneinue to sleep, isn't it?
What happens to the Coulomb Counter in such case ?
If we have a Culomb Counter deadband that does not allow detecting the 5mA, I presume the Coulomb counter does not count any energy flowing out of the pack, and due to the sleep mode only the Electronics Load is taken into consideration (plus the Self Discharge %): is that understanding correct ?
If instead we lower the Coulomb Counter deadband below 5mA, does the gauge count correctly the real coulomb being drained from the battery even if in Sleep Mode ?
Thanks a lot.
Pietro