This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5009: LM5009 rebootstrap issue

Part Number: LM5009
Other Parts Discussed in Thread: LM5019, LM5164, LM5163

Dear TI expert,

Application Description

1) 75VDC Vin  --> LM5009 buck (output 14V) --> LDO TPS70933 (output 3.3V)

2) LM5009's load are feedback resistor (47K+10K)  and LDO (3~4mA). 

Issue Description

Step 1: When 75VDC Vin switches off, LM5009's output 14VDC signal  s dropping slowly due to the load is light.

Step 2: When LM5009's output 14VDC signal  is dropping at 2.5VDC, 75VDC Vin  switches on again, LM5009 can't rebootstrap  due to LM5009's output 14VDC signal  is not zero.

Finally, LM5009's bootstrap pin keeps as 6.5VDC and LM5009's output 14VDC signal keeps as 2.5VDC steadily.

My question:

1) Even if LM5009 is at the Gate drive UVLO status, there is still a small current goes to load ? If yes, how much of this leakage current or discharge current ?