Other Parts Discussed in Thread: TPS2121
Hi Team,
we use the TPS2124YFPR to supply our device with either 5V from the buck converter itself (12V car battery supply to 5V) or from a USB 5V supply.
The switching between the supplies works, but if s supplied by both supplies at the same time, and then turning off the 12V car supply, the device resets.
As shown on the attached scope image the VOUT of the TPS2124 drops to 3.3V for around 100ms. The 4.0V RESET Monitor resets the whole system.
Please find the schematic below.
We use the TPS2124 in VCOMP mode. The 5V from the buck converter has priority as it can supply higher current (2A) then the 5V USB supply (700mA)
5V_Buck = from car batt 12V –> 5V Converter
5VD_USB3 = 5V USB supply
measurement in scope_2.png attached.
CH1 (yellow) = 5V_Buck
CH2 (green) = 5VD_USB3
CH3 (blue) = 5VD
We expected that shortly before the X1 cursor, the output switches to VIN_B, but this seems to happens much later at Cursor X2-
Could the reason be Hysteresis/Prio on VIN_B? Would it then be better to have 5V_Buck on VIN_B and 5V_USB on VIN_A?
Thanks,
Alen