Other Parts Discussed in Thread: TPS23523, TPS23521
Sir / Madam,
We are using TPS23521EVM-001 unmodified along with a Power Supply targetted for compliance and did a surge test.
The Power Entry connector has a TVS Diode AK15-066C-Y for surge protection, the link to the datasheet is below.
I am referring to the Section 3 : Description which says "The 200-V absolute maximum rating makes it easier to survive lightning surge tests (IEC61000-4-5")
The surge test -500V, +500V, -1KV, +1KV surge did not affect the board.
However, -2KV surge test caused the circled Diode (D2) of to fail as a short, circled below.

Refer the picture of Figure 1, page 3 of the document SLVUB67.
When this shorted diode was removed, we confirm there was no other shorting components.
I understand that this diode appears to be a "Freewheeling" diode for the inductor L1.
Below is the summary of the setup and outcome.

Below is the capture for the surge waveform at the instance for failure :

I would like to know what caused the Diode D2 failed to a short ?
I would like to know what the exact purpose of L1 and D2 are ? Can L1 be replaced with a short and D2 be replaced with a second TVS diode ?
Thanks,
Rajesh