Other Parts Discussed in Thread: TPS54233
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "FR9202T" ?
VIN max: 17V
Iout max: 2A
AEC-Q100 qualified
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "FR9202T" ?
VIN max: 17V
Iout max: 2A
AEC-Q100 qualified
Hi Kygo
Sorry for the delay. TPS54233-Q1 is good but I am wondering if the FR9202 is the AEC-Q100 qualified? And also, TPS54233 is a little bit over spec to compete with 17V device and it has SOIC package with non-sync topology. I would suggest TPS62130-Q1.
Here I have a few questions:
1. What is the customer and what is the application and its TAM?
2. Does customer care about P2P solution? Is there any requirement of the package?
3. What is the input, output and load current of the application?
4. Is there any special concern here? Such as load transient performance (note that TPS54233-Q1 uses CM control and the competitor uses COT control which means that the COT may get better transient performance ), thermal performance, etc..
Thanks.
BR
Ruby