This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17309Q3: Exposure of silver or silver plating

Part Number: CSD17309Q3
Other Parts Discussed in Thread: ADC082S021

There is silver (Ag) in Leadframe of target products.
Is the silver (silver plating) exposed?

-Target products
ADC082S021CIMM/NOPB
CSD17309Q3
CSD17581Q5AT
SN74LVC2G06DCKR
TPD1E1B04DPYR
TXS0102DCUT

Best Regards,

  • Hello Suzuki-san,

    Thanks for the inquiry. I am the applications engineer for TI's FET product line that includes the CSD17309Q3 and CSD17581Q5AT. You are correct that there is silver (3.25%) in the lead frame. The plating on the leads is tin (Sn) and there is no exposed silver (Ag). You can see this in the product folder under the Ordering & quality tab. You can get detailed material content by clicking on View or download under Quality, reliability and packaging information. I will forward this onto one of the other product teams for other devices in your list.

    Best Regards,

    John Wallace

    TI FET Applications

  • Hello, 

    This information is available online for most devices, I suggest using John's steps to find this information for the devices. If the information is not available, then I suggest posting about that part.  This will be quicker then trying to get each device checked as different groups within the company will need to be reached. 

    You can see this in the product folder under the Ordering & quality tab. You can get detailed material content by clicking on View or download under Quality, reliability and packaging information

    The lead frame is Tin as well on the ADC082S021. 

    Regards

    Cynthia 

  • Thank you for yuour answer.
    I have a question.
    If silver is used in the lead frame but the plating is other than silver (eg Tin), does that mean the product's silver is not exposed?

    Is it common to the following products?
    ADC082S021CIMM/NOPB
    SN74LVC2G06DCKR
    TPD1E1B04DPYR
    TXS0102DCUT

    Best Regards,

  • Correct, the plating will not allow for any exposure of the material underneath. 

    Regards

    Cynthia