Just want to make sure i understand how to read MON11 for UCD9090-Q1.
Based off of this link it sounds like you can only read MON11 as current or temperature (link). Is that true?
Assuming that is true then they just need to follow the following link (SLVA385) and refer to section 4.2 or 4.3? Based off the "Select the Rail" section of 4.1 - MON11 = PAGE10? Is that also correct?
Regards,
Kevin