Other Parts Discussed in Thread: LP5569
am trying to follow this example
Period 0x9f PSC0
Period 0x1f PSC1
Duty cycle 0x3f PWM1
def lp3944_dim_set_period(self, dim0_or_dim1: boolean, period: int) ->int: psc_reg = LP3944_REG_PSC0 if dim0_or_dim1 else LP3944_REG_PSC1 # Convert period to Prescaler value */ if (period > LP3944_PERIOD_MAX): return -1 psc_value = (period * 255) // LP3944_PERIOD_MAX psc_dim = "PSC0" if dim0_or_dim1 else "PSC1" print("Period " + str(hex(psc_value)) + " " + psc_dim) err = self.lp3944_reg_write(psc_reg, psc_value) return err; def lp3944_dim_set_dutycycle(self, dim0_or_dim1: boolean, duty_cycle: int) ->int: pwm_reg = LP3944_REG_PWM0 if dim0_or_dim1 else LP3944_REG_PWM1 # Convert duty cycle to PWM value */ if (duty_cycle > LP3944_DUTY_CYCLE_MAX): return -1 pwm_value = (duty_cycle * 255) // LP3944_DUTY_CYCLE_MAX pwm_dim = "PWM0" if dim0_or_dim1 else "PWM1" print("Duty cycle " + str(hex(pwm_value)) + " " + pwm_dim) return self.lp3944_reg_write(pwm_reg, pwm_value)