Hello Wenhao,
I saw that my issue was closed due to inactivity from my side. I was not able to look into the problem because of other activities. A short update:
- I checked the waveform at pin 5. It has always a high voltage, no drop or unwanted switching when enable pin connect to GND. I conclude that the TPS is really turned oFF and not switching
- Separated the TPS circuit from the load and measured the current into pin5. I measure 8,5uA (EN=0, In=3V). This current should be much lower.
After checking so many TPS61220 parts and looking at the data sheet, I can say that this current is the leakage current of internal switching FET (body diode). I will send the barcodes (on the tapes) to Ti customer service to check whether they are genuine or not.
Thanks for the feedback regarding the layout. I will implement your suggestions in next revision.
Kind regards,
Yilmaz