Other Parts Discussed in Thread: UCC29002,
Hi,
I am designing a power supply module with universal- AC input and 100W,35V output. I have a paralleling requirement for this AC-DC power supply, which means if needed user can parallel these 2 to 3 modules together to increase the overall power output or to increase the reliability of the power supply modules.
but i also have a hotswapping requirement for N+1 modules parallel redundancy solution. for this requirement I could see UCC29002+TPS2412 ic combination to achieve the parallel and redundancy solution.
since my output bus voltage is 35VDC, i can UCC29002 for this voltage level, but for TPS2412 in datasheet it is mentioned to use Controls Buses From 0.8 V to 16.5 VDC only.
how can I use this TPS2412 ORing power rail controller for this 35VDC bus voltage? is there any reference design for this voltage level for tps2412?
Thanks.