I have tried testing the LM5169 using the above mentioned EVM board.
What I see is that the primary output is stable even with no load but the secondary side is very dependent on the load. The board is equipped with an 1k secondary load which gives a nice and stable 10V as expected.
But changing this load in either direction makes the voltage rise and drop significantly. Lower load makes output voltage rises up to twice the set voltage and higher load makes the voltage drop more or less linearly.
What is the reason for this?