A similar question has been asked before about the Offline version and the answer was that the Export function is not available in the Offline software only the Live mode. Well I am running in Live mode and I do not see the export fuction.
Have FDPD Version 7.7.1 installed. USB Adapter or eval board attached. UCD90160A installed in the socket of eval board.
I have created a System File of 15 power rails in the UCD90160A. I have even proven that this works in an actual application.
Problem: I want to use a configuration file to program many other UCD90160A devices that are loaded in different locations (different PMBus Address) but have the exact same configuration. Since the FDPD will not allow a board to be programmed with a system file if the address doesn't match, I have searched for other ways to do this and found that it seems the best way to deal with this is to export an XML file and use this to configure my devices of varying address values.
The documentation "Configuration Programming of UCD Devices.pdf" says 4.1 Export Using the Fusion GUI The Fusion GUI is normally used to export device configuration data. To begin, you select Export from the File menu:" However I can't find any "Export" sub/menu anywhere in the Live app.

I have tried Live Mode, Offline Mode, EVAL board, Application board, USB to Eval, USB Interface Adapter, and several other combination and options. I can not find any way to export an XML file.
My Question: How do I export the XML file?