This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: What is the error range of the voltage read by the BQ27Z561 fuel gauge IC?

Part Number: BQ27Z561

Hi, expert

Using the BQ27Z561 fuel gauge IC, where can I find the error range of the IC's reading voltage in the specification?

For example:

actual voltage: 3600mV,

IC read voltage: 3600±5mV.

  • Hello Scofield,

    It is not possible to give a blanket statement for the error range since we use firmware to help with ADC calibration so many of the errors in the datasheet are reduced.

    Estimation can be made using the information in the datasheet, section 6.11 Analog Digital Converter (ADC)

    Sincerely,

    Wyatt Keller