Hi Sir,
Datasheet shows V(A)-V(C) Threshold for fast reverse current blocking is typ. -4mV, does it mean the ideal diode mosfet turns off in condition that 2A reveres current flow through mosfet (Rdson 2mohm). If my understanding is correct, does below scenario happen possibly?
Use two LM74810-Q1 for the dual PSU input in OR-ing connection and PSU has no sink current capability, . Is there possibility that ideal diode can't turn off since the reverse current is quite low? Another case, if one of PSU is disconnect suddenly, the ideal diode will not turn off since there is no reverse current flow (Input becomes high-impedance)?
We'd like to know the behavior of LM74810-Q1 base on our experience of other supplier's solution.