Other Parts Discussed in Thread: TINA-TI, LM61480, PSPICE-FOR-TI, LMR43610-Q1
Our IT Department just installed TINA-TI on my laptop today 5/06/2022. I have several designs on the TI WEBENCH Power tool involving DC-DC converters. When I click on the Export button in the upper right of the WEBENCH screen, I then get the option to export to TINA-TI. A small Tab at the bottom of the page appears with starting download. Every time after approximately 5 to 10 seconds, The small Tab displays "EXPORT FAILED" I have tried several times with the same result. Any help would be greatly appreciated. The Texas Instruments DC-DC converter being simulated is LM61480QRPHRQ1. The input voltage is set to 20 - 36VDC, The output voltage is set to 5.0VDC. The output current is set to 430mA. I have tried the online WEBench tool for simulating of the Input Transient response and the output voltage shown never reaches the desired set voltage of 5Volts. I believe the reason is because the time axis on the WEBence tool is not adjustable and if it was allowed to run long enough, the voltage would indeed reach 5Volts. That is why I had our I.T. department install TINA-TI as the simulation time is supposed to be adjustable. I know that the device that I am using (LM61480QRPHRQ1) is an 8A device but the data sheet states that it will operate at an output current of 0 to 8 Amps. I have two issues: 1. Why does the design (shown) not export into the Texas Instruments simulation tool TINA-TI, and 2. I would like a Texas Instruments FAE or representative to confirm that the LM61480QRPHRQ1 will indeed operate and is stable at relative low output currents since the WEBench tool does not confirm this, (as low a 0 Amps ,as the data sheet states). Thank you.
Stephen Gilbert