Hi,
One of my customers sent me an electronic board that was stuck in reset. After investigation, I found that the reset cause is a TPS82130.
I use a TPS82130 to produce a +3.3 V voltage (1.2 A) from a +12.0V voltage.
See picture below:
The PG output is used as reset source on my electronic board.
My issue is that the TPS82130 seems to start normally, but its PG output has a strange behaviour, causing burst of resets.
Here is what I see (PG output is no more connected to the rest of devices, except to the pull-up resistor).
CH1 is Enable input of TPS82130.
CH2 is Vout of TPS82130 (3.3V).
CH3 is PG output of TPS82130.
At the end of the Vout ramp, the PG signal leaves the 0V level for a 0.68V level, and ~2ms after reaches 3.3V and then falls to 0.68V.
PG voltage never goes to 0V (signalling a default), but does not keep a 3.3V level.
The Vout voltage is stable. If I don't use the PG as reset source, my electronic board behaves normally.
Do you have an explanation for the behaviour of the PG pin ?
I use many TPS82130 on my board without problem (I even have a second one that also produces a 3.3V supply from the same +12.0V input without problem).
Best regards,
Fred.