Good Day,
I am using an LM27222 as two half bridges in a full bridge amplifier scenario.
As of right now I'm trying to diagnose a single half bridge. I am using the sample circuit from the datasheet:
Where R1 is 1.5 OHM, C1 is 3.3uF. Q1 and Q1 have a gate capacitance of 10nF and the bootstrap is 0.33uF. According to common practice it seems acceptable to select a bootstrap capacitor that is greater than 10 times the gate capacitance of the FET and the input capacitance should be 10 times greater than the bootstrap capacitor. Which the circuit meets.
I have a separate digital circuit that is the "controller" and the switching frequency at 20kHz at a duty cycle of 50%. However, this burst of pulses occurs at a 10 percent duty cycle (The input to the amplifier is Low when this occurs). I've also tried a standard 50% duty cycle at the same frequency and the LM27222 still does not switch as expected.
What other issues would cause the IC to not switch at the high and low side switch? The bootstrap capacitor voltage at CB (Pin 3) referenced to ground, still seems to be too low (< 3V) and I'm not sure why this is as it seems as though there is plenty of capacitance.
Many Thanks,
Tyler