Hello,
I hope you are well.
We have implemented the TPS23753EVM-004 onto one of our designs but it doesn't seem to work as expected. The input seems stable enough when powered (screenshot 1) but on the output we can only see about 0.6V (screenshot 2) and the switching FET overheats. I've probed the gate of the FET and the voltage swing is excessively large (screenshot 3).
I have traced the schematic twice and I can't see any differences between the development board and our design. Could you please review the screenshots below and let me know if you have any ideas as to how to debug this? I'm happy to send our schematics on a private ticket.
Thank you.
Kind Regards,
Lou