Hi,
I am using the BQ76942. During testing, the 8 cells under test drifted apart 3.1 -3.75V triggering the permanent fail. The cells have been brought back into balance and after multiple power disconnects from the battery, PF Resets and Resets that have been issued to the board, the PF stubbornly refuses to Reset. As you can see there are no errors that would cause a PF enable following a reset. has anyone else seen this problem?
Thanks for your help in advance,
Richard