I have a 5V input and a 3.7-4.2V input
Using the Highest Voltage Operation mode, the start-up is not consistent.
Using the 23.7K and 5K for the 5V on IN1 what will the recommended resistor values be for the 3.7-4.2V on IN2 be?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a 5V input and a 3.7-4.2V input
Using the Highest Voltage Operation mode, the start-up is not consistent.
Using the 23.7K and 5K for the 5V on IN1 what will the recommended resistor values be for the 3.7-4.2V on IN2 be?
Hello Koos,
If you're using Highest Voltage Operation then there's no resistor dividers to set.
Usually increasing input/output capacitance helps significantly with the transition from one input to another, but it's a balancing act.
If you're trying to use priority mode now with FSW - we do not have any specific recommendations for the resistor dividers for each input level; however, I would suggest looking at the E2E FAQ posted below to help with seamless switchover. Just ensure that PR1 < 1.06V when you want IN2 to take over.
If you're noticing supply swinging (continuous switching from one input to the other) then adding input/output capacitance can also help, but adding hysteresis as noted in the FAQ linked below will also significantly help.
Regards,
Kalin Burnisde